10/28/2020 3:56 PM | |
Joined: 9/27/2006 Last visit: 9/27/2024 Posts: 12283 Rating: (2685) |
Hello Bert02; This article from Siemens Support provides an excellent analysis of the use of routers to connect different subnets in Profinet IO networks: Is cross-subnet PROFINET IO communication possible? https://support.industry.siemens.com/cs/ww/en/view/109479139 The "normal" way to connect 2 different subnets in a TCP/IP network would be to use a router, it can connect communication partners over distinct subnets. However...this quote from the document is to the point: “PROFINET communication via router is not possible; this means that real-time communication between both IP subnets is not possible” Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/28/2020 15:58:32 |
|
Follow us on