10/28/2020 3:12 AM | |
Joined: 9/9/2014 Last visit: 8/28/2024 Posts: 75 Rating: (0) |
Hi forum user, i found error code 0x0E6A when using FB P_SND_RK with CP341 in modbus RTU master protocol format. After checking manual "S7-300/S7-400 Loadable Driver for Point-to-Point CPs: MODBUS protocol, RTU format, S7 is master" edition 09/2009 error code listed for event class id 14 (0x0E) only listed event number until 103 (0x67) no information found in manual for event number 106 (0x6A). Anyone have same experience and issue for this error code? Do you have updated manual for the modbus master protocol? i have looking in the search portal, no newer manual listed. Thank you Attachmenterror_data.zip (106 Downloads) |
Follow us on