11/24/2020 6:28 PM | |
Joined: 3/28/2014 Last visit: 1/10/2024 Posts: 1 Rating: (0) |
I also need the VPN adapter to show up in the PG/PC Interfaces. With PST i can select this VPN and see my devices (configured or not) but this works with the PC/PG Interface selector from the one in control panel, also used by the older Simatic Manager. Why is that not possible anymore in TIAP ??? However i can see the TeamViewer VPN adapter in the list.. Making online connection to the plc is indeed not a problem by just selecting another interface. Anyone have a taught over how the adapters are selected to show up in the TIAP PC/PG list ??? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/25/2020 09:36:05New subject after splitting |
|
Follow us on