1/17/2021 4:41 PM | |
Joined: 4/25/2008 Last visit: 7/2/2024 Posts: 2 Rating:
|
Hi I have a situation where the Cp441-2 has modbus slave is installed in S7400h rack and communication is established Now I want to change the protocol parameters of CP441-2 in S7 400h rack In run mode .ist possible and for me if communication effects due to change in Cp441-2 is ok but the S7 400h redundancy shouldn't effect after download Thanks in advance.... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/18/2021 12:45:14New subject after splitting |
|
Follow us on