5/31/2022 12:47 PM | |
Joined: 8/21/2021 Last visit: 12/4/2023 Posts: 1 Rating: (0) |
Hello everyone, I have a new project where I need to control an electrical actuator with a FESTO CMMO controller the communication protocol for the controller is MODBUS TCP/IP I know it's possible to control it using an S7-1200 CPU from SIEMENS or equivalent but what I'm looking for , is to know if it's possible to control it using a LOGO 8 via LAN cable ? Can a LOGO support Modbuus protocol ? LOGO8 ref : 6ED1 052-2MD08-0BA0 Attached file ( Commissioning of CMMO-LKP in ModbusTCP ) thank you , AttachmentCommissioning of CMMO-LKP in ModbusTCP mode via TIA Portal .pdf (397 Downloads) |
5/31/2022 1:03 PM | |
Joined: 12/18/2014 Last visit: 7/13/2024 Posts: 33336 Rating: (4134)
|
No, this isn't possible with a LOGO!. |
Follow us on