9/10/2010 5:16 PM | |
Joined: 10/9/2007 Last visit: 10/8/2024 Posts: 1250 Rating: (115) |
Hi Ensark2 I've seen this problem. I don't know if it happens with all kind of devices and if this still happens, because the test was done 2 years ago. When you change something in ABB configuration, no matter if this has relationship with the communication/information to 61850, the compatibility keys are changed and you should again export CID from ABB and update it into Sicam. It seems that this behaviour may be avoided, but I don't know how. You can see what's the actual Compatibility key in any kind of device using our IEC Browser (www.siprotec.com). Just connect to the device and search for the keys. Maybe I have a picture showing the key from an ABB device, I'll look for it. In Sicam PAS Configuration go to Templates/IEC61850 and click on your ABB device. In the panel where you can see the information there is a panel or buttonon the right (or upside) side called Properties. Click on it and you'll see the compatibility key currently configured in PAS. Here you can also see the path you have to go in ABB via IECBrowser, which is something like IEDNAMECtrl/LLN0/DC. There are several of them (depends on the device) and all of them must be the same on PAS and ABB. Mike J |
Energy Automation products: Sicam, Siprotec, Digsi |
|
This contribution was helpful to1 thankful Users |
9/14/2010 8:47 AM | |
Joined: 11/18/2009 Last visit: 10/15/2024 Posts: 262 Rating: (18) |
Hi Mike J, I was able to find compatibility key in SICAM PAS, but when
AttachmentPrint Screen.pdf (1307 Downloads) |
9/15/2010 8:53 AM | |
Joined: 11/18/2009 Last visit: 10/15/2024 Posts: 262 Rating: (18) |
Hi Mike J, IEC Browser reads all atributes. Only I can't find compatibility key on
I send you CID and SCD files in attachment.
AttachmentSCD and CID.zip (1007 Downloads) |
Follow us on