5/8/2017 9:13 AM | |
Posts: 25 Rating: (0) |
Thanks for reply, I have make some more pictures about my program. You can see in the pictures my hardware configuration and some settings i have made. If i want to create a TCP subnet there is something i think is not correct like you can see in the pictures. I hope you can see on the pictures what i have already try and maybe you can see what i have done wrong. I have invite some pictures of difference way i try to send data to the printer. Thank you, AttachmentPictures.zip (309 Downloads) |
5/8/2017 10:37 AM | |
Posts: 25 Rating: (0) |
Thank you very much for fast reply, On the other side i have a Sato CL4NX printer and this work with difference protcol like (SBPL,SZPL,SIPL,STCL,SDPL) i think. I have also put the missing pictures in the attachment i have like you can see in the pictures set the partner on the IP adress of the printer also i have set the port on 9100 i have found this port in the settings of the printer. And thank you for the tip with using hyperterminal i'm gone download a program and test it and let you know what i get on the aplication. AttachmentTCP.zip (293 Downloads) |
5/8/2017 2:23 PM | |
Posts: 25 Rating: (0) |
Hello, I have try to work with hyperterminal but i don't recieve anything. I have make more pictures of what i have done. Maybe i forget something. I have also work with counters on done en error so i can see how many times they have already set and i see that i have a lot of errors and also a couple done. But stil i don't recieve anything. I hope you can help me AttachmentHyperterminal.zip (270 Downloads) |
5/9/2017 9:08 AM | |
Posts: 25 Rating: (0) |
Hello, I have never work with some programs like hyperterminal. So i don't know of everything is correct. On the laptop that i used i have found an other program (Windschark). And on this program i can see there happends something between PLC and Printer but i can't see what. Like you can see in picture 1 and 2 you can see there happends something between PLC (IP10.128.40.1) and printer (IP10.128.40.2). In picture 3 and 4 you can see what happens between then but i don't understand this. I hope you can. Thank you, AttachmentWindschark .zip (131 Downloads) |
Follow us on