5/3/2016 1:51 PM | |
Joined: 5/26/2011 Last visit: 1/10/2024 Posts: 455 Rating: (7) |
Good day expers! There's a S7-312 with CP341 (1CH01), which is communicating to a MODBUS device, which suddenly became faulty (has SF) upon start up from normal stop due to maintenance. The diagnostic buffer of CP341 says module not available (i/o access error or parameter assignment error). Usually what does this mean? They are requesting for programmer assistance, but I'm hesitating it's on the software side because they have no way to access the program. I think it must be a hardware fault. They say that the SF LED is steady and there's no Tx and Td LED anymore. Also, how can we make sure that the CP341 is not broken? I've read there should be a dongle inserted on the CP at the back for it's proper function? Would it be true for this particular device? Please see attached file for more detail. Thanks! AttachmentService Report - AGUS 6 Hydro Plant.docx (351 Downloads) |
Last edited by: G_R_E_Y at: 5/3/2016 1:53:41 PMLast edited by: G_R_E_Y at: 5/3/2016 1:54:42 PM |
|
5/3/2016 2:58 PM | |
Joined: 5/26/2011 Last visit: 1/10/2024 Posts: 455 Rating: (7) |
Hello Duris! Thanks for your prompt response. I'm not actually the author of the report, but yes I have the uploaded backup (please see attached), and yes they don't have the original project (so also no symbols!). When I tried to check the HWconfig the first time I saw that "Parameter" button on the CP properties, but it's greyed out and unclickable, I think I'm missing what is called a "parameter assignment software" on the manual. Can you also give me a link for it? But in any case, the system is running for quite some time already and then suddenly this happened without them having any access to software, so I doubt it is on the configuration. In any case, I look forward to your further response, thanks again! AttachmentAGUS.zip (384 Downloads) |
Last edited by: G_R_E_Y at: 5/3/2016 2:59:36 PM |
|
5/3/2016 5:02 PM | |
Posts: 3093 Rating: (323)
|
Hello Grey, 2) yes CP 341 parameter assignment tool 4) yes 5) I think so. Regards,
|
This contribution was helpful to1 thankful Users |
5/3/2016 5:28 PM | |
Joined: 5/26/2011 Last visit: 1/10/2024 Posts: 455 Rating: (7) |
1) So how is this being implemented? 2) Tnx for the link! 3) I see. How to determine if this (driver lost due to power and battery off) is what happened? Would it result on the CP341 diagnosis above (not available/io access or parameter error)? Also how do you reload the driver? Would it be enough to simply redownload an Step 7 program for it? 4) I see, thanks. 5) I actually mean something like wire break. But if the CP is broken would it also give that diagnosis above? Actually how exactly could we know if the CP is broken? Thank you very much for your answers to my *** questions, I'm really new to this and this is urgent. Looking forward for your further reponses. |
Last edited by: G_R_E_Y at: 5/3/2016 5:30:39 PM |
|
5/3/2016 5:37 PM | |
Joined: 9/27/2006 Last visit: 5/30/2024 Posts: 12257 Rating: (2669) |
Hello Grey; I have no opinion on your problem at this time, with the information provided, except that you could be facing a module failure (after long use) and you might have to think of replacing the CP (see your question 4 below). In the meantime:
Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on