4/19/2012 1:27 PM | |
Joined: 12/14/2010 Last visit: 5/9/2024 Posts: 116 Rating: (0) |
Hi, Seperate modbus library block available for s7-400 plc with CP341.copy the same and insert into |
4/22/2012 1:25 PM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Hello Vinesh, Just I want to add something, Can you tell me Which PtP version You have & also Modbus Master. Becasue in one of the project I have face problem because of not updated Driver, So Please Download the Latest Driver From Here. As you mention you can't downlaod driver Becasue of the Plant Running, So Checked the Version Also. |
Ammy |
|
This contribution was helpful to1 thankful Users |
4/23/2012 9:17 AM | |
Posts: 13 Rating: (0) |
Ammy The ptp version is V5.1.1
and today i will try upgrading as well as the firmware But do u have a sample program for my requirement with 2 slave devices? |
4/23/2012 10:03 AM | |
Posts: 557 Rating: (64) |
Hello, When you install CD i think you will get Sample program in SIEMENS library. Regards |
Follow us on