11/12/2015 9:52 AM | |
Posts: 112 Rating: (0) |
Hello expert I have a CPU 315-2DP with hardware configuration like in photo. Sometimes I have a problem with I/O and the CPU goes to Stop with I/O error on diagnostic buffer. This problem occurs once a week or maybe more. Have any chance that this problem caused by the PROFIBUS stations because the PROFIBUS cable is not on the good condition? Best regards Adi ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/12/2015 10:36:54 AMNew subject after splitting |
|
11/13/2015 10:18 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi Adi, we had already a discussion about this error. CPU 315-2DP, sometimes goes to STOP mode and turn on the SF ledis it the same CPU? and the same behavior?regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
11/13/2015 11:11 AM | |
Posts: 112 Rating: (0) |
Thanks for your answer Yes is the same behavior, but now my question is, have any chance that profibus cable cause this error? Regards Adi
|
Follow us on