4/10/2016 6:32 PM | |
Joined: 5/12/2006 Last visit: 8/27/2024 Posts: 22346 Rating:
|
Hello, try this: http://www.socomec.de/files/live/sites/systemsite/files/SCP/6_gestion_energie/diris/DIRI0948v3.gsd Last link scroll down to GSD Files.
Christoph |
This contribution was helpful to
2 thankful Users |
4/10/2016 7:10 PM | |
Posts: 107 Rating:
|
Thanks for your help, but when i try to install this GSD file in the Hardware Configuration, I receive attached error message |
4/10/2016 7:39 PM | |
Joined: 9/27/2006 Last visit: 8/27/2024 Posts: 12279 Rating:
|
Hello Mohamed; When you need to insert a gsd file from a 3rd-party, you cannot have the Hardware Configuration accessing other files of this type. In other words, please close the project window ("Test" in this case), but leave the HWConfig window open (without open project). Then try to insert the new gsd file. One this is done you can reopen the Test project window and continue with the Profibus configuration. If you need more information, follow the step^s in this FAQ: How do you integrate a GSD file into the STEP 7 HW Config for PROFIBUS or PROFINET? https://support.industry.siemens.com/cs/ww/en/view/2383630
Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 4/10/2016 7:43:18 PM |
|
4/10/2016 8:06 PM | |
Posts: 107 Rating:
|
I have closed the Simatic Manager but it didn't help and gives me the same error message. |
4/10/2016 8:51 PM | |
Joined: 5/28/2008 Last visit: 8/27/2024 Posts: 4515 Rating:
|
Hello Mohamed, Please follow Daniel & Christoph instruction to close your project. You need only HW config to be opened and close the project opened in it. Here's in detailed step by step of how to integrate gsd files: How do you integrate a GSD file into the STEP 7 HW Config for PROFIBUS or PROFINET? |
Ayman Elotaify |
|
Follow us on