1/28/2015 10:07 AM | |
Posts: 11 Rating: (0) |
Hello Bizz, the CM1542-5 (6GK7542-5DX00-0XE0) is a Profibus-Module. So you can't communicate via ethernet. Why not connect directly to the CPU 1513? regards |
1/28/2015 10:18 AM | |
Joined: 10/7/2011 Last visit: 3/6/2024 Posts: 28 Rating: (2) |
The device CM 1542-1 is in ethernet but the CM 1542-5 is in profibus |
1/28/2015 10:32 AM | |
Joined: 6/12/2012 Last visit: 2/8/2024 Posts: 165 Rating: (6) |
Hello! IBH softec has hardware that can convert the Profibus to ethernet.
|
Thanks, |
|
1/28/2015 10:40 PM | |
Posts: 11 Rating: (0) |
like i said, it should be possible to connect the CPU 1513 directly to the customer network via ethernet. |