9/24/2007 9:23 AM | |
Posts: 324 Rating:
|
Hi there, isn't it funny... I do not see anything with USB there... only Express Card, strange isn't it. Stay calm. |
11/24/2008 2:06 PM | |
Joined: 12/6/2006 Last visit: 7/8/2024 Posts: 92 Rating:
|
Dear mamssass, U can use CP5711 Card Please find the Details of the card with the attachment AttachmentCP5711.pdf (456 Downloads) |
Last edited by: CS Moderator at: 11/24/2008 5:04 PMpersonal data from a siemens employee deleted |
|
11/28/2008 6:11 PM | |
Posts: 19 Rating:
|
Hi everyone, I have just bought a Notebook HP Compaq 6730b (it has serial port RS232C; OS XP Professional SP3) and DuelAdapter. It works with CP5512 properly (CP5512 (PPI) with MicroWin and S7-200 so far). Only one problem is, that I have to insert DuelAdapter with the CP5512 after switch-on of the Notebook. When I switch-on Laptop with DuelAdapter inserted, CP5512 is not activated. I am going to test this configuration with WinCC Flexible and TP177B panel next week. I have problem with an WinCC Flexible installation (SQL Server installation failed). V.Slovak Thevia company Czech Rep. |
12/8/2008 5:22 PM | |
Posts: 19 Rating:
|
Hi, I have problem with MPI a DP protocol; CP5512 + DuelAdapter + HP 6730b does'nt work with panel TP170B Mono V.Slovak Czech Rep. |
Follow us on