5/30/2007 9:29 AM | |
Posts: 324 Rating: (30) |
Hello Dec, thank you for this information... I really appreciate this. Stay calm. |
5/30/2007 5:03 PM | |
Joined: 12/19/2006 Last visit: 2/6/2024 Posts: 5 Rating: (0) |
Hello,
We use ModbusTCP with PCS7 (S7-400 and S7-400H controllers) We purchase a driver block MODBUS from I&S "OPEN MODBUS/TCP no. 2XV9450-1MB00". The block supports Modbus function code 3 (read registers) and 16 (write registers). The block can be used both as client (modbus master) or server (modbus slave). We use the CP 443-1 (both ISO and TCP/IP), have not noticed any conflicts and the data through put is high (compared with the serial CP solution). In case our client only support RTU we could simply add a converter (DIGI ONE 70001777). http://www.industry.siemens.de/IT4Industry/EN/solution_services/SIMATIC_Addons/proto_mod.htm?PIdent=1075&SIdent=1003&TIdent=1016&QIdent=1025 Regards Robert |
Follow us on