4/16/2018 10:52 PM | |
Joined: 4/13/2018 Last visit: 11/16/2022 Posts: 7 Rating: (0) |
Hello, we have in our plant the system described in the attached file. in fact , each CP has its own IP Address 192.168.0.1 and 192.168.0.2 and test this with ping in cmd and the result was ok. Our problem is when we want to see accessible nodes in step 7, an error message appeared like in the attached image (sorry it's in french: please look to second reply) and it said that impossible to establish online link because the module don't have yet an IP address. And as you can see, only the mac address are shown. AttachmentArchitecture plc.pdf (67 Downloads) |
Last edited by: Sfaxien at: 4/16/2018 10:58:25 PM |
|
4/16/2018 10:56 PM | |
Joined: 4/13/2018 Last visit: 11/16/2022 Posts: 7 Rating: (0) |
This is the message: |
4/17/2018 12:27 PM | |
Joined: 5/12/2006 Last visit: 10/14/2024 Posts: 22411 Rating: (3017)
|
Hello, which router? Christoph |
4/17/2018 12:35 PM | |
Joined: 4/13/2018 Last visit: 11/16/2022 Posts: 7 Rating: (0) |
Hello Chris, the router is Moxa EDS-20B. |
Follow us on