3/26/2014 10:19 AM | |
Posts: 13 Rating: (0) |
Hi all, please I'd like to know a very simple way to connect my 220 cc three-phase motor, with a s7 300 via a Profibus network. Thank you
|
3/27/2014 8:31 PM | |
Posts: 13 Rating: (0) |
Please, can someone tell me if my diagram (in attachment) is right ?? I don't know which device use in the red case... |
3/27/2014 8:48 PM | |
Joined: 2/19/2013 Last visit: 5/10/2024 Posts: 184 Rating: (8) |
Sice you connect it to a Scalance, it has to be a Profinet device. |
3/27/2014 8:58 PM | |
Posts: 13 Rating: (0) |
ok, a profinet device. Please, which drive can I use for a Profibus instead the scanlace ? |
3/27/2014 9:08 PM | |
Posts: 8946 Rating: (999) |
PC and Touchdont need an adaptor if you have profinet. You can connect the ethernet interface of Panel and PC to profinet. |
3/27/2014 9:54 PM | |
Posts: 13 Rating: (0) |
Ok. I just wanna use one technology, profinet OR profibus but not both.
|
4/1/2014 10:35 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello Maryan, It depends on what you use, if you use the ET 200M modules you need SM 321,SM322,SM 331,SM332,if you use the ET 200S modules has its own modules. SIMATIC ET 200M Interface Modules - Distributed I/O ... - SiemensSIMATIC ET 200S - Distributed I/O SIMATIC ET 200 - Siemens |
Last edited by: Ste39 at: 4/1/2014 10:40 AMLast edited by: Ste39 at: 4/1/2014 10:37 AMLast edited by: Ste39 at: 4/1/2014 10:37 AM |
|
This contribution was helpful to1 thankful Users |
Follow us on