4/1/2014 4:32 PM | |
Joined: 7/29/2008 Last visit: 5/3/2024 Posts: 96 Rating: (4) |
I am using for the first time SCALANCE S612 (V4) and Softnet Security Client (V4+HF1). I would like to access a SIMATIC PLC/HMI network (NETWORK ID 192.168.3.0) remotely through VPN with a static IP using a router with portforwarding to s612 (UDP 500, UDP 4500). After following tutorials with no success. http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=22056713&objAction=csOpen&lang=en&siteid=cseus&aktprim=4&extranet=standard&viewreg=WW http://support.automation.siemens.com/WW/llisapi.dll?query=22056713_S612_VPN_DOKU_V30_en&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx&lang=en&siteid=cseus&objaction=cssearch&searchinprim=&nodeid4=20229805 SCALANCE S612 cannot be reached remotely through internet even through the security configuration tool online mode. WAN IP static address router IP 10.30.130.1 SCALANCE external IP 10.30.130.40 SCALANCE internal IP 192.168.3.210 Attached are pictures from the security configuration tool (V4). As for VPN tab, Wait for partner (responder) is selected and the WAN IP address is the public static WAN address. Any help will be greately appreciated.
Attachmentscalance_config.pdf (401 Downloads) |
4/3/2014 4:35 PM | |
Joined: 7/29/2008 Last visit: 5/3/2024 Posts: 96 Rating: (4) |
I did use wireshark but did not capture any ISAKMP packets. What does this mean?
|
5/12/2014 9:33 AM | |
Posts: 1368 Rating: (126) |
No, that firewall rule is not necessarry for building up a VPN. For the firewall/ Portforwarding http://technet.microsoft.com/en-us/library/cc779912(v=ws.10).aspx Please have a look at this Getting Started. In Chapter "Remote Access with SCLANCE S and SSC" the procedure is explained step-by-step https://support.automation.siemens.com/WW/llisapi.dll?aktprim=0&lang=de&referer=%2fWW%2f&func=cslib.csinfo&siteid=csius&treeLang=en&groupid=4000002&extranet=standard&viewreg=WW&nodeid0=18703650&objaction=csopen Perhaps, you should proof, if all steps are done in your configuration... A few more questions: On which PC SCT is installed ? PC with SSC? The Router, the SSC is connected is without VPN function? Sorry for the many questions: Your Problem is sth like finding a needle in ahaystack. |
3/7/2016 2:41 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by AutoGen_746386 is split to a separate thread with the subject Scalance S612, error whenever I download. Best regards |
Follow us on