3/28/2015 4:26 AM | |
Posts: 3 Rating: (0) |
hi all, im trying link s7 -1200 with Profcae Hmi by ethernet , but i can't find Proface Hmi to add network.... cpu 1214c (214-1hg40-0xb0) proface gp4301tm. tia V13 |
3/28/2015 8:21 AM | |
Posts: 3 Rating: (0) |
thanks Williamooow. can you show me "link the PLC with the HMI" in the Step7 program .. thanks... |
3/28/2015 9:04 AM | |
Posts: 3 Rating: (0) |
thank William , but you don't understand my question.. my problem is conect s7-1200 and HMI proface (gp4301) by ethernet (TCP ) commmunication... |
3/28/2015 11:07 AM | |
Posts: 5225 Rating: (1188) |
..okay. Nice picture. Have a look at.. http://www.pro-face.com/otasuke/files/manual/gpproex/new/device/sie.htm there is a link to the attached file. Something that you need to know - a device does not need to show on the network diagram in "Network View" under "Devices & networks" to be able to link to another device. If the HMI is in the same IP range as your PLC, then it can link to the PLC. From the attached document it seems that the HMI uses the native communication for the S7-1200 (please have a look). While you are waiting for someone whom actually work with the combination of hardware to answer you - have a look at.. You have to make sure of the hardware configuration of the S7-1200 is correctly set. * Ensure the IP address and mask is set. Look at the Profinet name used. * (important) "PLC" >"Profinet interface" > "Advanced options" > "Port (x1)" > "Port interconnection" > Partner port"; ensure this is selected at "Any partner" and not one of the other devices in your project. * "PLC" >"Protection" (FW4 PLC) - be very careful which selections you make here. Some selections make the the HMI needs to send the PLC a password to establish communications. If the above is after-all helpful, please let me know (thanks). Attachmentsies7tcp.pdf (1147 Downloads) |
12/12/2016 7:46 PM | |
Posts: 7 Rating: (2) |
I am using the GP4114 of the GP4000 series. GP-PRO EX supports many PLC versions/manufacturers. |
Last edited by: Samk101 at: 12/12/2016 7:48:08 PM |
|
Follow us on