11/11/2016 10:24 PM | |
Joined: 6/21/2016 Last visit: 10/26/2023 Posts: 1 Rating:
|
I use a S7-1212C and TIA basic v13: I have a case where the example code in the "S7_1200-HeperTerminal-TCP" is very close to a part of the task. I have adapted the code for my test Plc S7-1212C and tested but connecdtion is rejected. I can not get to the point where I can test send or receive. The connection is not established ! ! I get "TCP connection error: 10061" I am attaching my version of the sample code and PDF print of the code and data blocks. Please can someone help. Is there something fundamentally missing in the configuration. I'm new to this programming With best regards Niels-Ebbe Riise AttachmentComm TCP CPU-HyperTerminal_V13_SP1_S7_1212C.zip (402 Downloads) |
Follow us on