4/24/2007 9:03 AM | |
Posts: 54 Rating: (0) |
Is it possible to have 2 way comms between; S7 417-4 / CP443-1 Advanced and AB PLC5 ? TIA |
4/24/2007 10:04 AM | |
Posts: 5822 Rating: (411)
|
Hello, well, there are some new Documents that may intrest you in this situation: Communication between SIMATIC S7-CPUs on PROFIBUS and Allen-Bradley Controllers via SST PROFIBUS Scanner Connection between PROFIBUS Subnets and DeviceNet by AnyBus-X-Gateways Communication between SIMATIC S7 and Allen-Bradley ControlLogix CPUs via Ethernet: Use of "Echochange" gateways I hope this will help. Best regards J_Bell |
4/24/2007 10:47 AM | |
Posts: 54 Rating: (0) |
thanks for the reply, The "Echochange" gateway seems to be the way forward. much appreciated. |