11/30/2020 1:56 PM | |
Posts: 2 Rating: (0) |
Hi, I'm on TIA portal V16 and i can't find a way to add festo's drive controllers in the hardware catalog. I want to add the CMMT-AS-V1 Thanks you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/01/2020 09:53:44New subject after splitting |
|
11/30/2020 3:09 PM | |
Joined: 9/27/2006 Last visit: 5/12/2024 Posts: 12257 Rating: (2666) |
Hello Danny; To integrate a Festo module (or any 3rd-party equipment) in a Step 7 configuration, it must have a Profibus or Profinet communication interface, and the accompanying GSD or GSDML file that allows integration in the hardware configuration. The following link will show you downloads for the CMMT Profinet from Festo, the first available package contains the GSDML file for the CMMT-AS...-PN model (required for Profinet exchanges). https://www.festo.com/net/sl_si/SupportPortal/default.aspx?q=CMMT+Profinet&tab=4 The screenshot shows what you can find if you click on the "File and Language versions" link for that module. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/30/2020 15:10:26Last edited by: dchartier at: 11/30/2020 19:01:20 |
|
This contribution was helpful to3 thankful Users |
12/1/2020 9:32 AM | |
Posts: 2 Rating: (0) |
Thanks a lot. This was life saving ! |
This contribution was helpful to1 thankful Users |