7/17/2014 5:35 PM | |
Joined: 7/13/2014 Last visit: 2/24/2022 Posts: 4 Rating: (0) |
Hello Fafner, Yes, the system is already in the standar a since show a better performance than the n. Attahced you will find the recording, I. The signal strenght seems to e OK.
Attachmentsignal_recorder_SCALANCE_W700_bajando.zip (204 Downloads) |
7/18/2014 7:12 AM | |
Joined: 3/20/2013 Last visit: 4/3/2024 Posts: 676 Rating: (44) |
P.S. Indeed: the signal trace looks good |
Best Regards, |
|
7/19/2014 12:08 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (308) |
Hello, According to the signal trace, it seems that the speed is not reduced to 12 MBps. I would do this. A slower rate means a less complex modulation (which in turn means a more reliabel transmission and less repetitions). I understood that you now run without iPCF, and that you have only one AP (no roaming required). In this specific context, I would set the "background scan mode"in the client on "disabled". And also restrict the client to the radio channel used by the AP ("use allowed channels only" in thetab "allowed channel".This wil bind the client more strongly to the AP (it will not searchfor another AP with a better signal every 5 sec as per default). If the automation network is connected with the overal network, I also agree with Fafner that you should check how many broadcasts/multicats comming from the rest of the network impacts the wireless connection. You could consider to protect the automation network with a small router/firewall like Scalance S602. Routers will not passbroadcasts between subnets. If you are working with a decentralized I/O behind the wireless client, the PNIO update cycletime of it must be set to values compatible with a wireless Rcoax transmission (which never runs as fast as a wired connection). By default Step7 uses 2 msec in HWconfig. With one client, increase it to 16 msec. Also for the failsafe part, the profisafe monitoring times of the decentralized I/O (see in HWconfig), and also for the Timeout times at the blocksF_SEND(DP or S7) if they are used, must be compatible with a wireless Rcoax transmission. There is a table (S7fcotib as XLS sheet) allowing to compute the recommended minimum times. http://support.automation.siemens.com/WW/view/en/25412441 |
Last edited by: jklm at: 7/19/2014 12:29 PMlink to S7fcotib Best regards |
|
7/21/2014 7:22 AM | |
Joined: 3/20/2013 Last visit: 4/3/2024 Posts: 676 Rating: (44) |
please have a look in your Access Points: Information -> WLAN -> Overlapping AP Are there entries? |
Best Regards, |
|
8/6/2014 10:47 AM | |
Joined: 3/20/2013 Last visit: 4/3/2024 Posts: 676 Rating: (44) |
Thanks for reporting your solution. |
Best Regards, |
|
Follow us on