10/29/2021 2:21 PM | |
Joined: 10/10/2005 Last visit: 8/29/2024 Posts: 1917 Rating: (136) |
Hello washburn4life, I think, S7T V4.2 SP4 is not compatible for Windows 10. For Windows 10 you need S7T SP5. Or otherwise, S7T SP5 is compatible for Windows 10 but not compatible for Windows 7 Professional, Ultimate and Enterprise. For Windows 7 was S7T V4.2 SP4 compatible. I recommend also to install the SP2 to STEP 7 V5.6: Service Pack 2 STEP 7 V5.6 / S7-Graph V5.6 SP2 / Service Release 2 STEP 7 Professional 2017 And after to install the hotfix 5 to STEP 7 V5.6 SP2: Download Hotfix 5 STEP 7 V5.6 SP2 / STEP 7 Professional 2017 SR2 Cicero |
Follow us on