6/10/2022 4:13 PM | |
Joined: 12/21/2018 Last visit: 10/18/2024 Posts: 3 Rating: (0) |
after add RTD module AI8*13Bit 6ES7 650-8AE60-0AA0 hardware in IM module. when i try to download in S7 400 cpu error show like this (D221) the system data for connection or routing are not valid, the clock parameters could have incorrect setting. can not load SDB 701. The system data can not be loaded to module CPU 410-5H-1A R0-SB of station boiler. Look under details or try to determine the cause for the problem using the diagnostic buffer of module. so, an error show in diagnostic buffer of that in attached pic. so please help me. Shubham mistry ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/13/2022 11:55:08New subject after splitting |
|
6/13/2022 11:58 AM | |
Joined: 8/21/2014 Last visit: 10/8/2024 Posts: 1024 Rating: (14) |
Closed cause question posted twice. The second thread with the subjectHardware not download in S7 400 cpu, even without compilation erroris published within the conferenceSIMATIC S7-400 / S7-400H / S7-400F /FH Best regards, |
My Forum is the place to personalize your profile, |
|
Follow us on