3/4/2020 8:35 AM | |
Joined: 10/5/2018 Last visit: 9/2/2023 Posts: 1 Rating: (0) |
After using TIA Portal Step 7 suddenly works like this. I can't test any existing project. Need help urgent. |
3/4/2020 11:58 AM | |
Joined: 7/9/2015 Last visit: 9/27/2024 Posts: 3949 Rating: (587)
|
Hi, which Version of Step 7 V5.6 do you use. Best to install Service Pack 2 and also check if you have installed PLC Sim V5.4 SP8. Download- Links: STEP 7 V5.6 SP2 / S7-GRAPH V5.6 SP2 / STEP 7 Professional 2017 SR2 Trial DownloadTrial Software SIMATIC S7-PLCSIM V5.4 SP8Regards, Towome |
|
|
10/27/2020 9:27 AM | |
Joined: 5/3/2012 Last visit: 11/8/2023 Posts: 1 Rating: (1) |
I have exact same problem now, did found any solution? All Siemens SW are updated to newest versions. |
10/27/2020 12:35 PM | |
Joined: 3/11/2019 Last visit: 9/6/2024 Posts: 1569 Rating: (289) |
Hello, on my system it worked with deinstalling the current version of PLCSIM V5.4 in the windows control panel. After that, restarted the pc and installed the latest version of PLCSIM V5.4 from the download. Deinstallation was necessary before installing the latest version (also if the latest version is already installed). Maybe this helps. Trial Software SIMATIC S7-PLCSIM V5.4 SP8 including UpdatesRegards
|
Last edited by: sancruz at: 10/27/2020 12:35:56Last edited by: sancruz at: 10/27/2020 12:38:36Feedback appreciated, please rate |
|
This contribution was helpful to2 thankful Users |
2/24/2023 9:42 PM | |
Joined: 3/9/2017 Last visit: 9/25/2024 Posts: 1 Rating: (0) |
Hi, what helped me was to repair the PLCSIM installation via the Windows 10 settings menu 'Apps and Features'. |
Follow us on