6/10/2011 2:41 PM | |
Joined: 4/13/2008 Last visit: 4/5/2021 Posts: 71 Rating: (9) |
Completely agree. High-cost notebook. And that's why users should got something more than the others and specialized for its tool... Here even for creating partition or disk image have to pay (Simatic PC Image/Partition Creator), while there is a lot of much better utilities free of charge. Completely weird policy IMO (offtopic). Ok then. I think it is only reverse engineering of EC settings left to do. In case of spare time (maybe some day :D ) I will start it. Of course will inform you all what I digged out. So far will install external quiet fan to not let EC lock down. It is the most effective solution regarding price/performance ratio. cheers, Zee |
Z-men's room |
|
6/10/2011 7:03 PM | |
Posts: 947 Rating: (45) |
Hi, zeemens field pg contains at least two sensors: temperature of the motherboard (chassis) - typically thermistor, and temperature of the CPU processor - thermal diode integrated with the chip. Termorezistormozhet degrade due to misalignment of the measuring bridge, the actual sensor and give the wrong temperature. Degradation of the diode unrealistic, I guess. Therefore it is necessary to evaluate / look thermistor placement on the motherboard. What's the thermal contact. And forgot to say earlier, you have to blow the radiator or other heat pipes. That blow, use a vacuum cleaner suction on the ineffective |
This contribution was helpful to1 thankful Users |
6/11/2011 1:31 PM | |
Posts: 947 Rating: (45) |
Hi see site www.overclockers.com. I thing, you will find a lot of useful information about the CPU cooling |