7/13/2021 9:37 PM | |
Joined: 6/10/2020 Last visit: 8/30/2025 Posts: 30 Rating:
|
Hello, I'm installing Scout v5.3 on win7 ultimate 64 SP1 (virtual machine) and Step7 V5.6 PS1.At the end of the installation, it shows "creating config files error failed" and the installation failed. This Win7 VM was using a Scout 4.4 and worked well. I checked the logs and it shows below. The log file is attached. Any idea what's reason for it? Thanks! ERROR: Function CallMkcfgdb, creating config files failed u7: CreateProcess: Command: C:\Windows\system32\taskkill.exe Parameters: /F /T /IM u7sprssx.exe Start: 13:10:11 ExitCode=0 End: 13:10:12 AttachmentInstallScoutLog.txt (561 Downloads) |
Last edited by: AutoGen_6548995 at: 07/13/2021 21:38:34 |
|
7/14/2021 5:02 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
check the logfile "C:\PROGRA~3\Siemens\Automation\Logfiles\Setup\mkcfgdb.bat_071321_122138_Log.txt |
7/14/2021 5:10 AM | |
Joined: 6/10/2020 Last visit: 8/30/2025 Posts: 30 Rating:
|
Thank you!! I have checked the log and at the end it shows below. What does this message tell us? The full log is also attached! 12:44:12 install_request -i -DV BES_IT_DVUmcBaseGen -PD BES_IT_UMCCpuS7 -y V3.2\u7bd0vax.ini succeeded! 12:44:12 processing file u7setup\step20\bi_dv_simotion_4_0.txt... 12:44:12 install_request -i -DV BES_IT_DVUmcBaseGen -PD BES_IT_UMCCpuS7 -y V4.0\u7bd0fax.ini failed! Method name: FinalMessage::~FinalMessage Line number: 4343 12:44:12 internal error 'doWork' Method name: processFile Line number: 3321 12:44:12 error calling processFile Method name: scanDir Line number: 3530 12:44:12 u7bt05ax.exe -scan u7setup failed! Method name: FinalMessage::~FinalMessage Line number: 4343 Error: Creating config-files for UMCInstallation failed u7: ... Checking this protocol: search for errors ... Attachmentmkcfgdb.bat_071321_122138_Log.txt (446 Downloads) |
Follow us on