11/12/2021 2:39 PM | |
Joined: 10/11/2006 Last visit: 9/8/2025 Posts: 6039 Rating:
|
Hello, 7-segment display The 7-segment display provides further status information in addition to the LED displays. https://support.industry.siemens.com/cs/de/en/view/109801510 8 Module in RESET state (RESET button pressed; overtemperature; faulty/ disconnected fan/battery module) Fan faults are detected by • A cyclic fan test • Or when the fan is switched on a malfunction is detected (fan does not turn or fan turns at too low a speed). State 8 is also displayed when a fan module is not connected at switch on. For further information, see "Special operating states". Middle segment of the "8" flickers Power-up of the SIMOTION D4x5-2 has failed Possible cause: Incorrect boot loader on the CF card Update this with SIMOTION SCOUT (see SIMOTION D4x5-2 Commissioning and Hardware Installation Manual Update boot loader of the CF card (Page 372)).
|
With best regards, |
|
Follow us on