2/2/2022 9:35 AM | |
Joined: 12/7/2017 Last visit: 6/14/2024 Posts: 8 Rating:
|
Hi Forum, I have a Simotion D435-2 controlling some Sinamic drives. The customer tells me that they power cycled the machine and since then our machine will not start. When we try to turn on the machine we continuously get technology faults across all the axis. Looking in the Sinamics diagnostic buffer most of the drive objects are returning cyclic data transfer errors. I have attached the log file. Can anyone advise on the corrective action here? Could something on the CF card have become corrupt during the power cycle? Thanks. AttachmentSINAMICS_Device Diagnostics.zip (539 Downloads) |
Follow us on