(0)| 2/8/2023 4:39 PM | |
|
Posts: 2 Rating:
|
Hi, Did you try that solution and work? If Yes, Do you think we can connect an S5 150 rack to a S5 1500?, at the end it is profibus DP Thanks in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/09/2023 06:19:29New subject after splitting |
|
| 2/8/2023 8:08 PM | |
|
Joined: 9/27/2006 Last visit: 12/26/2025 Posts: 12474 Rating:
|
Hello Frank; Turning an S5 rack of the S5-115, S5-135 or S5-155 families to operate as a Profibus slave (to any Profibus master, including S7 CPUs) requires an IM 308C in the rack, as a replacement for the S5 CPU, and a download (and integration in Step 7) of the gsd file for the IM 308C. We used to do this quite often with a S7-300 with a Profibus-DP integrated interface, at a time when the S5 CPUs were being phased-out. (a few years ago, yes). Look at the following document for information on this modification: https://support.industry.siemens.com/cs/ca/en/view/6883963 Now, you mention a S5-150 CPU This is a much older unit than S5-155Us, and I do not believe an IM 308C would be a possible solution. Could you confirm that you are working with a S5-150, and provide us with the CPU designation (or part number), that would help us determine if there is a Profbus-DP solution available for your equipment. Hope this helps, |
Last edited by: dchartier at: 02/08/2023 20:10:24 |
|
| 2/9/2023 6:16 AM | |
|
Posts: 2 Rating:
|
I found another alternative with the Vipa 306-1UE00, As I Understood, that IM installed in central or extension racks of 135U and 155U can talk Profibus DP with S7 400 and I guess should be possible with the S7 1500.
|
Last edited by: Jen_Moderator at: 02/09/2023 06:25:13Quote inserted. |
|
| 2/12/2023 4:01 PM | |
|
Joined: 5/6/2010 Last visit: 12/24/2025 Posts: 2042 Rating:
|
Hello, please think about the solution to change the S5 I/O against S7-1500 modules. End of the SIMATIC S5 product life cycle In the middle of the text you can find the link to 83557459_83557459_peripherieadapter_2019_en.pdf (2,4 MB) There you can find the necessary adapter. regards |
Follow us on