10/30/2024 1:55 PM | |
Joined: 10/30/2024 Last visit: 9/10/2025 Posts: 9 Rating:
|
Hi, I have the same issue with my RF160C. I try to reset it with a RF160C_RESET bloc but I it's giving error code : 1500 This error code is "Wrong parameterization of the RF160C" I use a Byte 122 IN/OUT module and my ID's are 264 and 265. I use 122 as GSD_IO Would you have an idea of what i'm doing wrong ? Thank's ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/30/2024 13:56:52New subject after splitting |
|
10/30/2024 3:13 PM | |
Joined: 10/30/2024 Last visit: 9/10/2025 Posts: 9 Rating:
|
I have a RF220R on X1 and nothing on X2. I have the RF160C_RESET bloc from 63969277_rf160c_s71200_1500_v14_lib_v16 Documentation about the lib : 63969277_RF160C_S71200_1500_TIA_V11_en.pdf (siemens.com) I didn't change the properties of the RF160C, I join a capture of the properties. Thank's |
Last edited by: AutoGen_2621519 at: 10/30/2024 15:14:39Last edited by: Moderator_Lan at: 10/30/2024 15:20:51link optimized |
|
10/31/2024 8:21 AM | |
Joined: 2/10/2015 Last visit: 9/12/2025 Posts: 144 Rating:
|
Good morning, if your're using a RF220R field_on_time needs to be 1 (maybe we're lucky and that's all). |
10/31/2024 9:34 AM | |
Joined: 2/10/2015 Last visit: 9/12/2025 Posts: 144 Rating:
|
Hi, the setting determins the RFID transponder. RF200 only supports one type. All of the settings can be found in the manual (chapter 5.2 "Parameter setting by means of GSD file") |
Follow us on