(2)| 3/27/2023 5:12 AM | |
|
Joined: 6/30/2014 Last visit: 10/27/2025 Posts: 476 Rating:
|
Good morning, maybe this FAQ will help you too: All the very best, SuperPippo |
Last edited by: Jen_Moderator at: 03/27/2023 12:29:53Link optimized. |
|
| 11/20/2024 5:46 PM | |
|
Joined: 7/12/2022 Last visit: 3/12/2025 Posts: 3 Rating:
|
Hello, I had the same problem, it seems that after the Office 365 the xlsx export in queries stopped working, only the xls export was working. When you choose xlsx export just do nothing. The problem seems to be that for this query xlsx export it needs the ODBC Driver for Excel 32 bits. So you need to install accessdatabaseengine 32 bits to be able to export the xlsx query. You are still able to export the xls but if you would like to reimport a query you need to use the xlsx. Since I'm working with an Excel 64 bits when I tried to install it running the accessdatabaseengine installation file I got an warning saying that my current version is 64 bits and the installation is aborted. What I did was to run the installation through command prompt using Silent mode, after that xlsx export in queries started working normally. Just run the command below in the command prompt in the file installation location directory to install in silent mode: Regards, |
This contribution was helpful to
|
|
Follow us on