(0)| 7/22/2025 8:26 AM | |
|
Joined: 8/3/2009 Last visit: 12/19/2025 Posts: 16612 Rating:
|
Hello AutoGen_5842151 If you use no the HD Image from the old PC you should first install the WInCC Runtime Advanced Software on the new PC. Then you have two options: 1.) Use the TIA Portal Project and transfer the WInCC RT Advanced to the new PC (starting the Runtime loader/StartCenter on the PC -> settings and then Transfer Mode) After that open PGPC Interface settings in the Windows Control Panel and set the S7ONLINE Accesspoint (or if you use not the default one in your TIA Project) to the correct networkcard.TCPIP.1 (If you have trouble with common loading you can also do an offline transfer ) 2.) you have access to the old HD-> then you can copy just the runtime files (the paths are defined in the runtimeloader settings) to the new PC in the defined folders that are also set in the runtime loader. also PGPC Interface has to be set. |
|
If this Information really helps, you could use the Rate function |
|
Follow us on