9/18/2025 12:21 PM | |
Joined: 3/12/2024 Last visit: 9/19/2025 Posts: 187 Rating:
|
Hello, thats a lot of questions I hope I can answer them all fulfilling your needs. 1. the IoT2050 itself can replace a PLC or not?
1a. if yes - how to connect relay's coils or relay's feedback contacts?
1b. if no - it shall be expanded by the SM- modules (up to 6) but which ones (instead of connection to an existing PLC)?
2. the connection through a vpn is possible with the device alone?
2a if yes - how to administrate vpn, firewall and functionalities?
2b. if no - can it be done via CloudConnect7 + ScalanceRouter? Or is there a PLC (S7) necessary?
3. If connected to a PLC - is it possible to connect it to any PLC (Beckhoff, Selectron, WAGO) and what are the limitations if not a S7 is used?
4. As the support is only through this forum - are there any training available from Siemens or 3rd parties?
5. Is it possible to use an open operation system (OSS)? which ones? what are the limitations of using OSS instead of a SIEMENS- Example_Image?
BR |
Follow us on