9/10/2014 2:50 PM | |
Joined: 4/14/2010 Last visit: 8/6/2024 Posts: 525 Rating: (11) |
Greeting, We wish to monitor and control the energy consumption of BTS site with Webase solution. I found following two information, 1st with Telecontrol Server Basic and 2nd with SMS direct GPRS configuration. This is monitoring and control the information cyclically from the Remote Station to the Central Station here is one central station and Bulk of the remote station will be (with TeleControl up to 5000) Can we perform the both task with one CP1242-7 (Web base Monitoring and text SMS) with 1st Telecontrol Server Basic solution or we need two CP with Seperate configuration as attached. We have selected following hardware and Software for this project, please advice is it suficiente or any thing else required. 1.} Power supply PM 1207 6EP1332-1SH71 2.} CPU 1214C DC/DC/DC 6ES7214-1AE30-0XB0 3.} CP 1242-7 6GK7242-7KX30-0XE0 4.} SINAUT ANT 794-4MR, rod antenna 6NH9860-1AA00 5.} Router with DSL Modem and Port Forwarding 6.} PC for WinCC Runtime 7.} SIM card for CP1242-7 8.} SIMATIC STEP 7 BASIC V12 SP1 6ES7822-0AA02-0YA5 9.} Telecontrol Server Basic 8 6NH9910-0AA20-0AA0 10.} WinCC Runtime Advanced V12 6AV2104-0BA03-0AA0 11.} static IP address by the provider Thanks. AttachmentDesktop.zip (68 Downloads) |
Last edited by: Sarfraz Bhatti at: 9/10/2014 2:54 PMMS |
|
Follow us on