(0)| 4/26/2008 12:04 PM | |
|
Joined: 4/6/2006 Last visit: 11/21/2025 Posts: 604 Rating:
|
Hello, In chapter 7 of the LOGO! Manual is sescribed how to put the LOGO! in transfer mode. Switching LOGO! to PC↔LOGO mode 1. Switch the LOGO! with/without display to STOP fromyour PC (refer to the LOGO!Soft Comfort Online Help),or select the ESC / >Stop command on a device withdisplay and confirm the entry with ’Yes’. When LOGO! is in STOP and online with the PC, the followingPC commands are accepted: - Switch LOGO! to RUN - Read/write the circuit program - Read/write the summertime/wintertime Link to LOGO! Manual:LOGO! |
|
Best regards, |
|
Follow us on