(2)| 10/20/2016 1:58 PM | |
|
Posts: 2 Rating:
|
Dear All, While Running the Collision using the Release manager, the attached error log file came, can any one guide to clear the error, or provide suggestion to clear the errors. Thank you, R.Poovannan. AttachmentComos_Log__2016_10_20__15_30_06_00.txt (697 Downloads) |
| 11/5/2016 12:38 PM | |
|
Posts: 2 Rating:
|
Dear Mr. Pippo, Thanks for the reply. Attached log file while Microsoft object debugger running in back ground. Still the same error is coming. We are not raised it. COMOS version 10.2 SP2 we usually create each WL for each user, after completion of work will release the the sub master layer, then while releasing the sub master layer to master this error came initially. This error is came in our data base. Issue is only in this particular layer only. Thanks in advance AttachmentSQL1-2.zip (666 Downloads) |
| 11/16/2016 2:57 PM | |
|
Joined: 6/30/2014 Last visit: 10/27/2025 Posts: 476 Rating:
|
Dear Mr. Poo, I had a look into the logs, but I cannot say what the source of the issue is, as this needs a deeper investigation. Also, the usage of the Forum should not substitute the Support-Tools. In your log I see that the used Comos Version is 10.1 SP2. Could you please open a ticket at the Support of COMOS for this? With best wishes, SuperPippo |
Follow us on