(0)| 6/26/2008 9:48 AM | |
|
Posts: 156 Rating:
|
Hi cep dedi,the project you got from your vendor is engineered with SCOUT V3.2.In order to be able to work with this project in SCOUT V4.0 the project format has to be converted up to V4.0. But only the data content of the SCOUT project is converted to V4.0, not the SIMOTION device version.After that, choose "opened write-protected" if you only make debugging activities. But you can change the write protection later on if necessary.Please have a look to the documentation SCOUT_configuring.pdf (V4.1) (http://support.automation.siemens.com/WW/view/en/27002825)In Chap. FAQs > Handling Recommendations for Service with SCOUT V4.1, you can find a detailed description about that, which is also valid for SCOUT V4.0.Best regards Manfred |
Follow us on