(0)| 4/3/2018 9:51 AM | |
|
Joined: 5/16/2016 Last visit: 12/19/2025 Posts: 92 Rating:
|
Hi, Hope it´s ok I insert my own question regarding S7 configuration here. I was thinking about presenting an Int as decimal value in Desigo CC. As far I can see there is only the Real object that can present a decimal value? It´s quite common in integrations into the predecessor to Desigo CC that values are presented as Int values and then XX amount of digits are presented as the decimal. Best Regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/3/2018 11:32:49 AMNew subject after splitting |
|
Follow us on