(1)| 3/30/2012 1:04 PM | |
|
Posts: 3037 Rating:
|
Hello, Do you use an adapter from USB toRS232 to the download? The downloadwith RS232/PPI Multi-Master cabledoes work only with a real RS232 interface. You can see this in the following FAQ. What transfer options are available in the various operator panels? You can do a download about MPI/Profibus. If the panel have an ethernet interface, you can do a download about ethernet. You can see the settings of the RS232/PPI Multi-Master cable in the following link attachment 4 > chapter 1.2. How do you do an operating system update (OS update) on operator panels? Tweety |
| 8/23/2019 11:04 AM | |
|
Joined: 3/16/2016 Last visit: 1/16/2024 Posts: 22 Rating:
|
Same problem, any help?? |
Follow us on