(0)| 3/10/2020 9:40 AM | |
|
Posts: 7 Rating:
|
Thanks for your help. Check attached project. AttachmentS7_Test_.zip (724 Downloads) |
| 3/23/2020 11:24 AM | |
|
Joined: 10/3/2008 Last visit: 10/22/2025 Posts: 996 Rating:
|
Hi, the example projects are installed with the setup: https://support.industry.siemens.com/cs/ww/en/view/109752686 (older version) or The bit CONN_ESTABLISHED only shows, that the connection is established, not that telegrams are transferred. When the S7 is the client, a positive edge of ENQ_ENR starts a telegram. When the telegram is finished with DONE or ERROR, you can set the next positive edge on ENQ_ENR to start the next telegram. Have a look at the block online help or the manual. In this the functionality of the block is also described. Wüstenräuber |
Follow us on