(0)| 9/14/2020 12:04 PM | |
|
Posts: 5 Rating:
|
The problem is when I start WinCC Flexible Runtime with current project which is working normal another HMI panel, it’s showing “Project id area pointer: unknown error” message on the above just 2, 3 second, sometimes “Connection failure” alarm appearing 2, 3 second on the start (please see attachment). I listed my actions on the below. - Checked IP addresses. Primary controller: 10.1.3.150, secondary controller: 10.1.3.151, HMI 1(which is working normally): 10.1.3.152, new HMI: 10.1.3.153 - Pinging. New HMI panel windows is pinging normal with primary and secondary controller and HMI(please see attachment) - Checking project ID field from WinCC project (“0”) it’s the same with HMI 1(which is working normally) - Checking the DB address field from WinCC project it’s the same with HMI 1(which is working normally) - On the compilation progress output panel massage “Required license: WinCC Flexible / Archives PC-RT” (maybe it has something to do with it) - WinCC Advanced v13 installed in the new HMI but I installed WinCC Flexible Advanced 2008 SP3 without uninstalling the WinCC Advanced v13 (because our project made in WinCC Flexible, we were not sure about migrating project) and it was first step If you can do any help for us I appreciate that, please do your best Sincerely,
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 09/17/2020 16:17:48New subject after splitting |
|
Follow us on