(1)| 11/18/2020 6:35 PM | |
|
Joined: 4/7/2012 Last visit: 7/10/2025 Posts: 37 Rating:
|
That's what I want, too, with only the DB2.DBW50 variable. This post I have 80 discrete errors (MW60, MW62, MW64, MW66, MW70 for example). Number 1: Error text 1 Number 2: Error text 2 Number 3: Error text 3 ... Number 70: Error text 70 If there are 3 error messages at a time, Error number: 10, M60.5 Error number 20, M70.2 Error number 70, M65.5 Thus, only the last error message is displayed due to one error line.But if the value of DB2.DBW50 changes, the number of errors specified by its value is displayed. DB2.DBW50 = 10 ---> then Error number 10: Error text 10 Timer 2Sec DB2.DBW50 = 20 ---> then Error number 20: Error text 20 Timer 2Sec DB2.DBW50 = 70 ---> then Error number 70: Error text 70 As long as error 3 exists, it cyclically alternates the text in a line which errors are currently active. It’s hard to describe, I’ll post a video and then what it’s all about. Thanks! https://support.industry.siemens.com/tf/ww/en/posts/how-to-make-a-cyclic-scroling-into-a-alarm-display/69558/?page=0&pageSize=10 |
| 11/18/2020 8:56 PM | |
|
Joined: 4/7/2012 Last visit: 7/10/2025 Posts: 37 Rating:
|
Here is the promised video Thanks! |
Last edited by: Jen_Moderator at: 11/19/2020 08:36:40Embedded video. |
|
| 11/18/2020 9:50 PM | |
|
Joined: 4/7/2012 Last visit: 7/10/2025 Posts: 37 Rating:
|
Thanks! |
Follow us on