9/11/2008 4:15 AM | |
Posts: 139 Rating:
|
you might want to have a look at the following site http://www.iba-ag.com/products/index.php?ptype=online&dlgroup=PDA&ID=802&level=3 these guys have products you can set up on the bus as a bus spy and grab the IO data as it comes across profibus etc. Also there arecards as well for direct connection to digitals inputs and analogs etc as well. with their equipment you can get sample rates down to 1ms. so have a look and see if there is anything you like or at least get some ideas of the type of gear you might like to use. |
9/24/2008 1:48 PM | |
Posts: 3 Rating:
|
Hi all, I've used PLC Analyzer from autem in the past to do exactly what asked,It's very easy easy to used and with the S7 driver is cycle precise http://www.autem.de/e_index.htm |
3/2/2010 11:09 AM | |
Posts: 2 Rating:
|
Who has used aVisor?Look like a good data collector. I need to read a lot of data each scan (5-10ms).
|
Last edited by: Stierlitz at: 3/2/2010 2:20 PMLast edited by: Stierlitz at: 3/2/2010 2:17 PM |
|
6/2/2010 6:55 AM | |
Joined: 10/7/2005 Last visit: 9/14/2025 Posts: 3049 Rating:
|
That's alright Krish, I'm happy to take care of this for you The ibaPDA S7-Analyzer is only one small powerful piece in the overall high speed data acquisition, storing and analysis related offering from iba. iba is also not limited to Siemens PLC related high speed data acquisition, but supports numerous PLC vendors, bus systems (the Profibus "Sniffer" ibaBM-DPM-S-64 being an all time personal favorite) as well offering direct hardwired "Parallel Analogue/Digital Units"(aka PADU's, with up to 25KHz sampling rate, i.e. every signal gets capturedevery40 micro seconds). Add synchronised high speed cameras capture,HMI screen capture,powerful reporting,its own active X embedded "Q Panel" mini HMI,etc. etc. to thatand you get a rough idea ofwhat iba can do (they've been around and active in the high speed data acquisitionmarket for over 25 years). As such any ibaPDA system is highly scalable and can comprise of onlya simple troubleshooting related S7 Analyser to begin with and "grow" to becomea Plant wide high speed data acquisitionrelated "Historian". Enough said (or advertised) and before someone tries to shoot me down in flames, I will officially declare a conflict of interest with my advise here as I am working for a company that also has a stakein www.iba-oceania.com (its excellent gear though, just take my word for it - andif you are interested in iba and arein theAustralasion region, please feel free to contact iba Oceaniaand ask for fritz). |
Last edited by: fritz at: 6/2/2010 7:30 AMLast edited by: fritz at: 6/2/2010 7:09 AMCheers |
|
Follow us on