3/15/2024 11:58 AM | |
Joined: 12/18/2014 Last visit: 5/17/2024 Posts: 33052 Rating: (4082) |
Solar Positioning Algorithm (SPA) Library for SIMATIC S7-1200 / S7-1500The "Solar Positioning Algorithm (SPA) Library" provides the calculation of the actual position of the sun for any location on Earth. The position of the sun is given in relation to the angles Azimuth and Zenith. Which can then be used to calculate the right angle for the Tracking movement This library can be universally used with the following controller:
|
Follow us on