7/12/2018 4:12 PM | |
Posts: 7 Rating: (0) |
Hello, Thanks for your quick response, I managed to upgrade the firmware of the CPU Controller, which is the V1.8 upd 5, but now I have another issue. When I start the CPU with the SW Controller, I should have the CPU configurated with his default IP address 192.168.0.1. But I don’t have this initialization, the SW Controller says that to set the CPU to RUN, I need to load the project into the CPU (see pictures 1 and 2). So, I tried to implement the TIA project in the CPU with TIA Portal V15 but I can’t establish a connection between the CPU and the Computer (see picture 3). Moreover, the RN led on the CPU doesn’t lighted up even when the CPU is in RUN mode. Do you have an idea how could I be able to make a connection between the CPU and the Computer? Thanks by advance. Regards Joévin AttachmentPictures.pdf (346 Downloads) |
7/20/2018 9:30 AM | |
Posts: 7 Rating: (0) |
Hello, Thanks for your response, I tried to perform a factory reset using the TIA Portal project view as you suggested but I have also troubles to do that. Indeed, when I search the PLC via the LAN adapter (or just with an ethernet cable), TIA Portal doesn’t find any devices (picture n°1) and therefore I can’t go online to perform the factory reset. I tried to see if the problem could come from something else, so I searched why the LEDs of the PLC was off (picture n°2) and the only explanation I could find was the one present on the picture n°3. I don’t know if this problem is linked with the software on the PC part of the ET 200SP because, as I said in my previous post, I performed an update of the Software Controller (V1.8 upd 5) and the only information that I have on this part is that I need to download a configuration on the CPU so I could put it in RUN mode (picture n°4). So the main problem that I have is that I can’t communicate with the PLC via TIA Portal. If you have any idea how I could restore the link, I will be grateful. Thanks by advance. Regards Joévin AttachmentPictures.pdf (321 Downloads) |
Follow us on