(0)| 5/7/2021 5:25 AM | |
|
Joined: 5/4/2021 Last visit: 12/15/2025 Posts: 3 Rating:
|
Hello bergmanu can you helpme to a little expalin, what i need to do after the hardware instalation of SImatic IO 6ES7-647-OKA01-0AA2 , I have devicewise installed in the board,DeviceWise( Telit) only says . "When the Siemens IoT 2000 gateway IO device is Started, variables will be accessible as device variables." The USER variable structure is available when a Siemens SIMATIC IoT 2000 I/O-Sheild is not attached, and theShieldparameter = None. "When the Siemens SIMATIC IoT2000 Gateway I/O-Shield is attached to the gateway and theShieldparameter = Siemens is selected from the device definition, the following additional device variables will be enumerated:" ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_1488357 at: 05/07/2021 06:58:48Last edited by: Jen_Moderator at: 05/07/2021 08:58:28New subject after splitting |
|
Follow us on