(0)| 8/12/2021 8:52 AM | |
|
Posts: 4 Rating:
|
I have one 1215 DC/DC/DC CPU Directly connected throw Ethernet Cable to media converter X101-1 .That X101-1 connected to other X101-1 via FO cable .PC is connected To other X101-1 via Ethernet cable. all Wire & Cable Found ok But Connection LED P1,P2 are not Glow .we also on Transfer Link Using Set Button, But No Led Glow ,also We Try change Setting BY pressing Set Button as said in Manual of X-101 point 4.4.7.but Problem Is not Solved .still No Led Glow in Both x101-1.there is no Fault in both x101-1 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/12/2021 09:40:50New subject after splitting |
|
| 8/12/2021 9:41 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject Scalance X101-1: LED P1, P2 are not Glow is published within the conference Communication / Networks. Jen_Moderator |
Follow us on