1/27/2022 12:09 PM | |
Joined: 6/19/2018 Last visit: 8/7/2025 Posts: 10 Rating:
|
I have an application where I will require the use of 4 servo motors. I have decided to use Sinamics V90. The application will be speed control only. I found two application examples, one that shows the setup using a hardware support package: and the same example, but using a GSD file: Position Control of SINAMICS V90 with SIMATIC S7-1500 via IRT PROFINET (using a G... - ID: 109739053 - Industry Support Siemens My question is which method is better? what are the advantage/disadvantages of using HSP or GSD? Software: TIA Portal V16 Upd2 CPU: 1515T-2PN Application is speed control only using Telegram 1 |
Last edited by: Jen_Moderator at: 01/28/2022 07:46:54Optimized links. |
|
1/27/2022 12:42 PM | |
Joined: 6/19/2018 Last visit: 8/7/2025 Posts: 10 Rating:
|
Thank you sir! |
Follow us on