(0)| 2/1/2022 5:08 PM | |
|
Joined: 1/17/2006 Last visit: 12/28/2025 Posts: 555 Rating:
|
Hello ! 1. In the selection of the motor encoder in the Sizer, for example, "AM24DQI - absolute encoder 24-bit + 12-bit multiturn", it means that if I adjust fine resolution p418=2 (2-bit) I will have 6 -bit for multiturn: 32 (maximum) - 24 - 2 = 6-bit for multiturn ? 2. And does 6-bit for multiturn mean that a maximum of 64 turns can be evaluated by the encoder? 3. So, the total resolution will be 26-bit (24-bit + 2-bit) = 67108864 ? Regards, Berg
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/02/2022 08:43:01New subject after splitting |
|
This contribution was helpful to
|
|
Follow us on